AXIS#.IL.COGCOMP.TEACH.ACC
Description
Sets the acceleration used during the Cogging Compensation teach.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-08-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: RPM See Acceleration Units for details. |
|
Range |
Depends on units. See Acceleration Range for details. |
| Default Value | 30,000 rpm/s |
|
Data Type |
Float |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL |
0x500A | 0x1F | UINT | 1:1 | Acceleration | RW | False |
| AXIS2.IL.COGCOMP.TEACH.ACC | 0x510A | 0x1F | UINT | 1:1 | Acceleration | RW | False |